EPD Extension Kit for MSP430 LaunchPad
 All Classes Files Functions Variables Typedefs Enumerations Enumerator Macros Pages
Functions
Uart_Controller.c File Reference

The functions to control and return system packets. More...

#include "EPD_Kit_Tool_Process.h"
#include "Uart_Driver.h"
#include "Uart_Controller.h"

Functions

void poll_system_packet_buffer (void)
 Polling data from system packet buffer.
 
void return_system_packets (system_packets_t *packet)
 Return system packet. More...
 
void return_packets (system_packets_t *packet, uint8_t *data, uint8_t len)
 Return system packet result. More...
 
void return_system_packet_result (system_packets_t *packet, uint8_t result)
 Return system packet result. More...
 
void data_controller_init (receive_packets_event OnRxPacketEvent)
 Initialize the UART data buffer and trigger receiving (Rx) packets. More...
 

Detailed Description

The functions to control and return system packets.

Copyright (c) 2012-2013 Pervasive Displays Inc. All rights reserved.

Authors: Pervasive Displays Inc.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Function Documentation

void data_controller_init ( receive_packets_event  OnRxPacketEvent)

Initialize the UART data buffer and trigger receiving (Rx) packets.

Parameters
receive_packets_eventFor trigger Rx packet
void return_packets ( system_packets_t packet,
uint8_t *  data,
uint8_t  len 
)

Return system packet result.

Parameters
packetThe address pointer of system packet
dataThe data byte will return
lenThe length of return data packet
void return_system_packet_result ( system_packets_t packet,
uint8_t  result 
)

Return system packet result.

Parameters
packetThe address pointer of system packet
resultSuccess or failure
void return_system_packets ( system_packets_t packet)

Return system packet.

Parameters
packetThe address pointer of system packet that will return